AXIS#.MT.FEEDRATE

Description

Use to dynamically change the speed of motion tasks while they are in motion. This is useful in applications like machine tooling where a manual over-ride may be present that can slow down or speed up a movement without stopping the machine, or stopping a sequence.

When the feedrate is changed, only velocity is scaled. Acceleration and deceleration are not scaled and maintain the value entered into the motion task.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Percent

Range

0.000 to 100

Default Value

100

Data Type

Float
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
AXIS1.MT.FEEDRATE

50d0h

01h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MT.FEEDRATE

51d0h

01h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MT.FEEDRATE

6311

18A7

Unsigned32

Read/Write

-

AXIS2.MT.FEEDRATE

71847

118A

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.FEEDRATE

6311

Float

Read/Write

-

Related Topics

Motion Tasks